When the input event occurs, the display switches to another visualization within one frame.
|
“Frame selection type” |
|
|
“Switch local visualization” |
The “Frame Selection” group is visible. |
|
“Switch to any visualization” |
The “Frame and visualization selection” group is visible. |
|
Requirement: “Switch local visualization” is selected. |
|
|
“Frame selection” |
List of all frames that contain the active visualization. The referenced visualizations are listed below each frame, as determined in the “References” property of the respective frame. Example: |
|
“Assign selection” |
The selection in the “Frame selection” input field is accepted. Then it appears in the “Selected frame” and “Selected visualization” settings. Requirement: A visualization is selected in the “Frame selection” input field. |
|
“Selected Frame” |
Name of the frame to be switched to Example: Hint: Use the “Assign selection” command for changing the setting here. |
|
“Selected Visu” |
Name of the switched visualization Example: Hint: Use the “Assign selection” command for changing the setting here. |
|
Requirement: The “Switch to any visualization” option is selected. |
|
|
“Frame and visualization selection” |
Contains the frame to be switched to |
|
“Assign” |
Frame to be switched to (with complete path). The index determines the visualization. Example: The path is specified in the following syntax: Caution: Visualizations can be nested at any depth by means of frame elements. In order to use the “Switch to any visualization” frame selection type without any problems, a frame must not contain more than 21 referenced visualizations. |
|
“Assign expression” |
Variable ( Example: |
|
“Index to select” |
Index that determines which of the referenced visualizations is displayed
Note: The referenced visualizations of a frame are indexed automatically according to their order. |
Requirement: The project contains visualizations that form a structure.